{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I create a Pointer to a memory words using SoMachine V4.3?
Below is an example for using the POINTER TO INT Instruction .
It can be used to move consecutive located Integer from a source to a destination.
In this example, it moves %MW0-%MW5 to %MW100-%MW105.
The Length determines the amount of memory words to move.




Schneider Electric Nigeria