{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
The Documentation window will not come up in the ProWORX 32 software.
Issue
Documentation window will not come up

Product Line
ProWORX 32

Resolution
The ProWORX 32 Documentation window is either minimized or hidden behind another window. Close down the ProWORX 32 software. Deleted the "layout.acf" and/or "layout3.acf" file(s) from the C:\Proworx\32 folder. This resets the ProWORX 32 windows to default. Relaunch the ProWORX 32 software and the Documentation window should now reappear.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top