{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
Issue:
Where can I find requirements and download the StruxureWare Data Center Expert desktop client software?

Product Line:
Struxureware Data Center Expert (DCE)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment:
Struxureware Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)

Cause:
In order to discover devices and do most of the configuration required for DCE, you need to download and install the client application to your local system.

Resolution:

System Requirements
Downloading

Minimum System Requirements for the DCE Desktop Client

Information! This article only discusses downloading and installing the Desktop Client for the Data Center Expert software.  For instructions on deploying the Data Center Expert Virtual Appliance on VMware or HyperV, see knowledge base Video: Data Center Expert | How do I download and deploy the Virtual Appliance? .

The Data Center Expert Desktop Client (console) is a stand-alone Java application that runs on systems that meet the following requirements:
NOTE: See therelease notes for the most up-to-date information on system requirements.
Downloading the Desktop Client



1) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.

2) In the upper-right corner will be an option to Download Client.
NOTE: In older versions, it may be on a different area of the web interface.

3) To continue you will need to Read and Agree to the license agreement.

4) Download the Binary.exe for the Desktop Client (application).

5) Run the downloaded executable file and follow the on-screen instructions.

6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation) or the Start Menu Option for Data Center Expert #.#.#.
NOTE: Starting with version Data Center Expert version 7.9.3, the Window's Desktop client is available for download from Upgrade and VM download pages.  The upgrade page can be accessed through the EcoStruxure IT Entitlements Portal.  If you are unable to access the upgrades via the EcoStruxure IT Entitlements portal, please reach out to your local technical support.

Schneider Electric Nigeria

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: