Search FAQs
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
Issue:
Where can I find requirements and download the StruxureWare Data Center Expert desktop client software?
Product Line:
Struxureware Data Center Expert (DCE)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
Environment:
Struxureware Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)
Cause:
In order to discover devices and do most of the configuration required for DCE, you need to download and install the client application to your local system.
Resolution:
System Requirements
Downloading
Minimum System Requirements for the DCE Desktop Client
Information! This article only discusses downloading and installing the Desktop Client for the Data Center Expert software. For instructions on deploying the Data Center Expert Virtual Appliance on VMware, see knowledge base FA299551.
The StruxureWare Data Center Expert Desktop Client (console) is a stand-alone Java application that runs on systems that meet the following requirements:
NOTE: See the release notes for the most up-to-date information on system requirements.
Downloading the Desktop Client
1) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.
2) In the upper-right corner will be an option to Download Client.
NOTE: In older versions, it may be on a different area of the web interface.
3) To continue you will need to Read and Agree to the license agreement.
4) Download the Binary.exe for the Desktop Client (application).
5) Run the downloaded executable file and follow the on-screen instructions.
6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.
NOTE: Starting with version Data Center Expert version 7.9.3, the Window's Desktop client is available for download from Upgrade and VM download pages. The upgrade page can be accessed through the EcoStruxure IT Entitlements Portal. If you are unable to access the upgrades via the EcoStruxure IT Entitlements portal, please reach out to your local technical support.
Where can I find requirements and download the StruxureWare Data Center Expert desktop client software?
Product Line:
Struxureware Data Center Expert (DCE)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
Environment:
Struxureware Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)
Cause:
In order to discover devices and do most of the configuration required for DCE, you need to download and install the client application to your local system.
Resolution:
System Requirements
Downloading
Minimum System Requirements for the DCE Desktop Client
Information! This article only discusses downloading and installing the Desktop Client for the Data Center Expert software. For instructions on deploying the Data Center Expert Virtual Appliance on VMware, see knowledge base FA299551.
The StruxureWare Data Center Expert Desktop Client (console) is a stand-alone Java application that runs on systems that meet the following requirements:
- A PC with a 1-GHz or better AMD/Intel processor running a 64-bit operating system: Microsoft® Windows® Server 2016 and 2019, Windows 10 and 11
- At least 2 GB of RAM and 20GB disk space
- Screen resolution should be set to at least 1024 x 768.
- Supported browsers: Edge; Mozilla® Firefox®; Google Chrome™ See Known issues in DCE for details about support for Internet Explorer and Edge
NOTE: See the release notes for the most up-to-date information on system requirements.
Downloading the Desktop Client
1) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.
2) In the upper-right corner will be an option to Download Client.
NOTE: In older versions, it may be on a different area of the web interface.
3) To continue you will need to Read and Agree to the license agreement.
4) Download the Binary.exe for the Desktop Client (application).
5) Run the downloaded executable file and follow the on-screen instructions.
6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.
NOTE: Starting with version Data Center Expert version 7.9.3, the Window's Desktop client is available for download from Upgrade and VM download pages. The upgrade page can be accessed through the EcoStruxure IT Entitlements Portal. If you are unable to access the upgrades via the EcoStruxure IT Entitlements portal, please reach out to your local technical support.
Released for:Schneider Electric Nigeria
Explore more
Product:
Range:
Explore more
Product:
Range: