{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum current rating of an ATS22 relay?
Issue:
Maximum current rating of an ATS22 relay.

Product Line:
Altistart 22, ATS22

Environment:
All

Cause:
N/A

Resolution:
Max switching capability:
5A - 250VAC or 30VDC on resistive load (p.f.=1)
2A - 250VAC or 30VDC on inductive load (p.f=0.4)

Schneider Electric Nigeria