Issue:
Wants to program the ATV61/71 drive to start/stop using terminals and use the HMI (keypad) as speed control.
Product Line:
ALTIVAR 61, ALTIVAR 71
Environment:
All
Cause:
N/A
Resolution:
Under drive menu, go to 1.6 [COMMAND] menu:
Set Ref 1 channel to HMI.
Set Profile to separate.
Set Cmd channel 1 to terminals.
Wants to program the ATV61/71 drive to start/stop using terminals and use the HMI (keypad) as speed control.
Product Line:
ALTIVAR 61, ALTIVAR 71
Environment:
All
Cause:
N/A
Resolution:
Under drive menu, go to 1.6 [COMMAND] menu:
Set Ref 1 channel to HMI.
Set Profile to separate.
Set Cmd channel 1 to terminals.
Released for:Schneider Electric Nigeria