{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What's the Com'X510 maximum memory expansion possible?

Article available in these languages: Thai

Issue
User would like to know why only 3.7GB's of data is shown on the COM'X510 snapshot, as well as, is the memory expandable.

Product Line
COM'X 510

Environment
Energy Server, Ethernet Gateway

Resolution
The SD Card in the COM'X 510 is actually a 4GB SD Card.  This card is used to store the historical data logged in the COM'X 510.
Data is automatically overwritten after 25 months, so logging less doesn't get you more time.
The amount of storage is equal to...32 devices, 30 topics each at 15 minute intervals = 25 months of data.

Schneider Electric Nigeria