Which port will L9_XMIT function block work with on the Unity 140CPU6xxxx
Answer
Issue The Unity help does not state which ports on the 140CPU6xxxx supports the L9_XMIT function block.
Product Line EcoStruxure Control Expert (formerly known as Unity Pro), Quantum
Environment Unity Pro v10, 140CPU67160
Resolution The Unity documentation shows the following statement for the XMIT block.but it does not specify the PLC type. The Unity 140CPU6xxxx only has two Modbus ports.
Function Description The L9_XMIT (transmit) function block sends Modbus messages from a master PLC to multiple slave PLCs or sends ASCII character strings from the PLC's Modbus slave port #0, port#1, or port#2 to ASCII printers and terminals. L9_XMIT sends these messages over telephone dial up modems, radio modems, or simply direct connection.
The L9_XMIT will only work with Modbus port 1 on the 140CPU6xxxx.
Released for:Schneider Electric Nigeria
Explore more
Range:
Modicon Quantum
Profibus DP Fieldbus
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.