{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Speed pot range for ATV212 Drives?
Issue:
Range of potentiometer used on ATV212 Drives.

Product Line:
ATV212, S-Flex

Environment:
All

Cause:
Need to select a speed pot.

Resolution:
The speed pot range is 2.2 to 10 KOhms. Can use the ATVPOT part number which is 2.5 KOhms speed pot.

Schneider Electric Nigeria