{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to update the variable by polling when NOP as IEC61850 client
There are two ways for the variable update in PLC when the NOP as IEC61850 client. One is polling, the other is report. Both of them need to be configured. This application present a configuration steps for the polling.

The detail of the steps can be referred the attachment.

Schneider Electric Nigeria

Attachment(s)
AN_PAC_LCZ_NOP VariablePolling_0.1.docx [82.57 KB]