{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PowerChute Network Shutdown 4.0 Fails to shutdown host containing VMware vMA and vCenter Server Appliance, when host is added in cluster with IP

Issue:
ESXi host that contains both PowerChute Network Shutdown (PCNS) installed in VMware Virtual Management Assistant (vMA) and vCenter Server Appliance (VCSA) and is added to cluster with IP (while configuring the cluster) does not shutdown.

Product Line:
PowerChute Network Shutdown 4.0

Environment:
Issue specific to scenario where VMware vMA and vCenter are on same host
OS: Any VMware ESXi, vMA and vCenter

Cause:
ESXi host running PCNS and vCenter Server VMs has been added to the Inventory using IP address instead of Fully Qualified Domain Name (FQDN)

Solution:

Uninstall PowerChute Network Shutdown 4.0 and install PowerChute Network Shutdown version 4.2

Or while setting up cluster, add hosts in vCenter with FQDN rather than IP to avoid this issue.

Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: