{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I configure an M580 PAC to log events to a syslog Server?
Goals and Symptoms
Syslog is a standard messaging service that can be used to monitor security and other events. It is available on the M580 using
Unity Pro version 10.0 or greater. The attached document  is a descriptive example of using syslog with Unity.

Facts and Changes
In a system using syslog the M580 acts as a client sending messages to a syslog server. Each message is time-stamped
and an NTP or SNTP server must also be configured. This example uses a BME P58 1020 PAC. The NTP server is a
TCSESM083F2CU0 Connexium switch. The syslog server is an open source server Visual Syslog. The configuration of each is
described in the attachment.

Schneider Electric Nigeria

Attachment(s)
SYSLOG .pdf [1.09 MB]