{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which cable reference can we use between TM3XTRA1 (TM3 bus extension transmitter module) and TM3XREC1 (extension receiver module)
The extension receiver module TM3XREC1  can be at  maximum distance of 5 meters  from the TM3XTRA1
The Catalog recommend to use  the references VDIP1845460xx;
VDIP184546005 (0.5 m)
VDIP184546010 (1.0 m)
VDIP184546020 (2.0 m)
VDIP184546030 (3.0 m)
VDIP184546050 (5.0 m)

But as these references does not meet the UL requirements , for US market machines installation needs it’s advised to use 2 other references:
490NTW00002U (2.0 m)
490NTW00005U (5.0 m)
which are UL rated


Schneider Electric Nigeria