{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMXART0414 appears to be consuming one additional register.
Issue
BMXART0414 appears to be consuming one additional register.

Product Line
BMXART0414

Environment
Unity, Control Expert.

Resolution
If you configure a BMXART0414 and an analog module (e.g.,  BMXAMI0810) with no gap in the state ram assignment between the
two modules, the first registers of the analog will appear not to work or overwritten.

The reason this occurs is because the BMXART0414 reserves one additional register for the cold junction.

The workaround is to allocate a one register gap between the two modules.

Schneider Electric Nigeria