{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to add the alarm severity to an alarm summary column in Vijeo Designer?
Issue:
Looking for an example on how to show the alarm severity in the alarm summary.

Product Line:
Vijeo Designer (all versions)

Resolution:
Currently there is no specific column that can be added to display the alarm severity in the alarm summary. The workaround for this is to do the following:

1) Add in the alarm message the alarm severity at the beginning of the message. For ex. [1]: This alarm is active.
2) In addition, set the Alarm Summary to sort by severity as well.

Schneider Electric Nigeria