{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Why is the dynamic braking resistor repeatedly failing in our lift application?
Issue:
Why is the dynamic braking resistor repeatedly failing in our lift application?

Product Line:
Dynamic braking resistors, Altivar 71

Environment:
Lifting applications 

Cause:
DBR failure

Resolution:
Generally, the dynamic braking resistors burning or failure happens due to higher braking energy dissipation than it's power rating.
If you select the normal braking resistor part reference provided in the catalog, the power rating of the resistor is insufficient to dissipate the braking energy generated by the motor in during downward movement. Hence it will burn the resistor due to overheating.

The lift is a vertical and cyclic movement application, and the braking power dissipation is similar to hoisting application. Hence it is necessary to select the hoisting resistor part references provided in the ATV71 catalog to avoid DBR failure due to overbraking.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.