{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum speed a VFD can safely operate a motor speed?
Issue:
Minimum speed the VFD can safely operate a motor?

Product Line:
ATV212, ATV21, ATV312, ATV12, ATV32, ATV66, ATV71, ATV61, ATV11, ATV58, ATV31

Environment:
All serial numbers

Cause:
N/A

Resolution:
The VFD can safely run to a motor to 0.01 hertz, however, the lowest speed is dependent on what the motor/application can handle.

Schneider Electric Nigeria