{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Modbus Plus tap assembly part# 990NAD23000 and the Modbus Plus part# AS-MBKT-xxx connectors be used on the same Modbus Plus network.
Yes. The only thing to take notice of is that the Modbus Plus tap assembly part# 990NAD23000 module sets termination by jumper settings whereas the ASMBKT-185 connector has a built-in termination and the ASMBKT-085 connector is non terminated for in-line connections.

Schneider Electric Nigeria