{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can the 2-wire type (TCT) parameter be found on the Altivar process drive?
Issue:
TCT parameter on the Altivar process drive

Product Line:
Altivar Process

Environment:
All models, All serial numbers

Cause:
Documentation

Resoultion:
Complete Settings-> Command and Reference-> 2-wire type

From the main menu, Navigate to "Complete Settings" then "Command and Reference".  From here, you can scroll down to 2/3 wire control, and if it is set to 2 wire, 2-wire control type can be found just below.

Schneider Electric Nigeria