Search FAQs
How to connect a Ethernet wire of section smaller than 1 square millimeter to the auxiliary connector in Okken 70-M and BlokSeT Mw2 ?
1. As the Ethernet wire is very thin, 0.5mm, before crimping it you need to bend it, as showed below
2. After that, you crimp it using the crimping tool in the 1 position (1mm)
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009I2PAQA0&oid=00DA0000000abSm)
3. This is the result
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009I2PBQA0&oid=00DA0000000abSm)
4. As the wire is very thin, in order to reduce the fragility of the wire, we recommend to protect the wire and terminal with a thermo-retractile glove.
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009I2PCQA0&oid=00DA0000000abSm)
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009I2PDQA0&oid=00DA0000000abSm)
2. After that, you crimp it using the crimping tool in the 1 position (1mm)
3. This is the result
4. As the wire is very thin, in order to reduce the fragility of the wire, we recommend to protect the wire and terminal with a thermo-retractile glove.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: