According to datasheet, operating distance is "50m", and maximum sensing distance is "100m". What is a difference between these distance explanation?
We speak about 100m in free field, we can guaranty a well functioning at 50m in industrial applications, actually it depends mainly of where the system is installed, for the moment no customer is complying about low range.
Released for:Schneider Electric Nigeria
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.