{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How small of a motor can be run with an ATS22 Soft Starter?

Article available in these languages: Spanish

Issue:
Motor be undersizing on an ATS22

Product Line:
Altistart 22

Environment:
All models

Cause:
N/A

Resolution:
The ATS22 is very tolerant to running small motors. It is designed to provide motor overload protection for FLA at least 40% of the softstarter rating.
Parameter (In) setting range is 0.4xIcL to IcL, with IcL being the softstarter's amperage rating.
If a smaller motor is used, an external overload relay should be used.

Schneider Electric Nigeria