{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does ramp increment mean for the Altivar 61/71?
Issue:
Ramp increment meaning for the Altivar 61/71.

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers

Cause:
N/A

Resolution:
Ramp increment is a parameter that will change the resolution of the listed parameters:  see below
Inr M [Ramp increment] 0.01 - 0.1 - 1 0.1
0.01 [0.01]: Ramp up to 99.99 seconds
0.1 [0.1]: Ramp up to 999.9 seconds
1 [1]: Ramp up to 9,000 seconds
This parameter is valid for [Acceleration] (ACC), [Deceleration] (dEC), [Acceleration 2] (AC2) and [Deceleration 2]
(dE2).

Schneider Electric Nigeria