{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the hardware & software requirements of SCADAPACK workbench and SCADAPACK configurator ?

The table below lists the basic hardware and software required to install and operate SCADAPack
Workbench and SCADAPack Configurator. If you are installing both applications, install them on a single
computer that meets the requirements for both applications. Additional requirements follow the table.


Table

In addition:

  • If the Microsoft .NET Framework 4.0 is not already installed on the computer, you will need an Internet connection to the computer so it can be installed.
  • If SCADAPack Workbench 6.x or the ISaGRAF Automation Collaborative Platform (ACP) 6.x is installed on the computer, remove it before you begin the installation.
  • If you download the SCADAPack Workbench software, store the files on your local computer in a directory with a path name that is less than 30 characters in total.

Schneider Electric Nigeria