{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can we achieve Trip circuit Supervision function in Masterpact Air circuit breakers?

Trip circuit supervision is not possible with Masterpact breakers because the coils used are not conventional magnetic coils but includes electronic components. Supervision is not possible with these types of coils because of electronic component inside the coil, which makes it difficult to achieve supervision function.

Schneider Electric Nigeria