Search FAQs
What is the typical response time for Sepam 80 Modbus protocol?
The Sepam Modbus protocol typical response time (time between the end of request reception and sending the reply) is less than 10 milliseconds for 90% of exchanges. It may occasionally be longer, but not exceed 150 ms. In indirect mode, the time needed between the request (or an acknowledgment) and the availability of the corresponding data is linked to the Sepam low-priority cycle time and may vary from a few dozen to several hundred milliseconds.
AEDL3
AEDL3
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: