{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where to locate the serial number of Sepam 20 and 40 base units?
Aside from acquiring the serial number of Sepam 20 and 40 base units via the front panel, SFT2841, or SFT SAV, it is also possible to acquire the serial number by looking at the base unit itself. Unfortunately, sometimes people get confused with the serial numbers of the other modules connected the base unit, for example the MES module.

For Sepam 20 and 40, the serial number of the base unit is printed on a sticker located on the right-side-face of the Sepam.

AEDL3

Schneider Electric Nigeria

Attachment(s)
ScreenHunter_84 Jan. 11 15.33.jpg [36.86 KB]