{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the CAN J1939 Protocol supported by SoMachine 4.1, 4.2 or 4.3?
The CAN J1939 Protocol provided by CODESYS and its Online Help documentation is delivered in a separated Add on that can be installed on top of SoMachine V4.1 SP2, 4.2 or 4.3. This protocol is  supported on M241/M251 controllers only. This add on is free of charge. It will neither be shared on SESU nor www.schneider-electric.com, only through ADEs, SAEs and customer support.

Schneider Electric Nigeria