Search FAQs
Is the S-Flex drive available in Nema 3R outdoor enclosure?
Issue:
Is the S-Flex drive available in Nema 3R outdoor enclosure?
Product Line:
S-Flex
Environment:
3R enclosure
Cause:
n/a
Resolution:
Yes, They are available in Nema 1, Nema 12, and Nema 3R.
Nema 12 and 3R units have a longer lead time because they are not stocked and must be built to order through product selector.
Is the S-Flex drive available in Nema 3R outdoor enclosure?
Product Line:
S-Flex
Environment:
3R enclosure
Cause:
n/a
Resolution:
Yes, They are available in Nema 1, Nema 12, and Nema 3R.
Nema 12 and 3R units have a longer lead time because they are not stocked and must be built to order through product selector.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: