Issue:
Can I get the VW3A3720 or the Ethernet module for the ATV630 Process drive?
Product Line:
Altivar Process 630
Environment:
All
Cause:
VW3A3720 availability
Resolution:
Yes, it is available and your ATV630 Process drive must be firmware version 1.5 or above to use this option card.
Can I get the VW3A3720 or the Ethernet module for the ATV630 Process drive?
Product Line:
Altivar Process 630
Environment:
All
Cause:
VW3A3720 availability
Resolution:
Yes, it is available and your ATV630 Process drive must be firmware version 1.5 or above to use this option card.
Released for:Schneider Electric Nigeria