In case relay works without problems software is not needed to be updated. But in case software update is needed contact vampsupport. Tell clearly the reason why update is needed. Inform also type and serial number of the relay.
Released for:Schneider Electric Nigeria
Explore more
Range:
Vamp Software
Vamp Measurement and Monitoring Units
Vamp Arc Flash Detection
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.