{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the batteries in an SYBT5 be replaced individually?
Issue:

This question is often asked by customers, especially by their procuring departments.  "Why are the internal individual batteries not replaced instead of replacing the complete SYBT5 battery module?".

Product Line:
Symmetra LX

Resolution:
APC by Schneider Electric does not recommend replacing the batteries or any part of the SYBT5 / SYBT5FR module nor approve replacement of the internal batteries for the SYBT5 / SYBT5FR by third parties, nor will APC by Schneider Electric provide any proprietary work instructions and/or spare parts used in the official assembly. If an SYBT5 / SYBT5FR module has already failed, replacing the internal batteries would not clear the fault on that module. It would still show as a bad battery.

The SYBT5 / SYBT5FR is unique in regards to how it communicates with the system of a Symmetra LX. There is a circuit board inside the module that is factory calibrated to the individual batteries. This provides the sophisticated battery management that the LX offers. The individual batteries in the SYBT5 / SYBT5FR are also produced by selected providers that adheres to the standards that APC by Schneider Electric gives them in terms of ratings and such.

Installing the internal batteries into an SYBT5 / SYBT5FR would require someone to reprogram the module with a proprietary calibration code from APC by Schneider Electric assembly areas. No one outside the manufacturing of APC by Schneider Electric will have the correct proprietary code nor the means to program or reproduce it in its entirety. This is only done by the facilities of APC by Schneider Electric where the battery modules are officially manufactured. This is done as to  ensure that all individual modules has been properly programmed and it will communicate all that is needed to ascertain that the intelligence modules reads the batteries correctly. The SYBT5 / SYBT5FR will then go to quality assurance tests before it is sold out to the market to assure full functionality. Failure to put in the right code and/or programming may cause adverse effects to the overall functionality of the Symmetra LX.

Because such reconditioned / refurbished battery modules may not communicate properly with the Symmetra LX System, as would be the case after such a replacement, various issues which could impair system operation and fault alarms may appear:
  • Battery charging issues may occur which can lead to critical system failures
  • Intelligence modules and/or Symmetra (XR) Extended Run Frame communication cards may not interpret the battery overall status correctly and may fail to support the attached load
  • APC by Schneider Electric PowerChute Shutdown Software may not properly work and improper shutdown to load droppage may be experienced
  • Added safety features like for the SYBT5FR will not present if the batteries were replaced or programmed incorrectly

As unauthorized modification of a component assembly voids the system UL/IEC/CE rating, the Symmetra LX unit may not be recertified and/or revitalized of its contract. APC by Schneider Electric will not provide support for such refurbished batteries, or any faults that occur as a result of batteries which have been refurbished in this way. Also, if the internal Battery Cells were replaced with single APC VRLA's but, done outside of APC by Schneider Electric official assemblies / factories or made without prior authorization from the company, APC by Schneider Electric, will not honor this, and will not replace the SYBT5 / SYBT5FR nor be responsible for faults and/or issues the Symmetra LX and any of its load may experience due to the use of improper and unauthorized SYBT5 / SYBT5FR assemblies.

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: