{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PowerChute Network Shutdown VM Prioritization web page displays "vCenter Server is inaccessible. Please verify that the vCenter Server IP/Hostname and logon credentials are correct."

Issue:
PowerChute Network Shutdown VM Prioritization web page displays "vCenter Server is inaccessible. Please verify that the vCenter Server IP/Hostname and logon credentials are correct."

VM prioritization page

Product:
PowerChute Network Shutdown v4.x, 5.x

Environment:
VMware ESXi

Cause:
Application times out while cataloging VMs.

Solution:

Edit the vmprioritization.js file to increase the time out.

If PowerChute has been installed to the default path on Windows OS, open C:\Program Files\APC\PowerChute\group1\comp\http\html\scripts\vmprioritization.js with a test editor like Notepad++.

search for the lines that include  "timeout". there should be two lines.

"html_data" : {
"ajax" : {
"url" : "/ajaxvmlist",
"data" : {
formtoken : jQuery("#formtoken").val(),
formtokenid : jQuery("#formtokenid").val(),
},
"type" : "POST",
"timeout" : 20000,
"success" : function(data) {
if (data === "99") {
jQuery("#vCenterConnectionError").show();
}

The default timeout value is 20000 or 90000. Change the value on both lines to 6000000.

After saving the changes to the file, you must clear the cache in the web browser (so that the cached js file is not used).

If PowerChute is installed on Linux, the default path to vmprioritization.js will be found in /opt/APC/PowerChute/group1/comp/http/html/scripts/vmprioritization.js

To verify the vCenter username and password in the PowerChute UI, go to Communications Settings.

Communications settings page


Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: