{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the purpose of the "FDR Synch" button in the BME NOC's DTM while using M580 HSBY System
In a HSBY system, the FDR servers of the paired BMENOC's are automatically synchronized.
You can remove the auto-synch by disabling this service in the DTM.
If, for some reason, you want to manually re-sync the servers, you can do it by pressing this button.
Note that it will also reactivate the auto-sync, as this is the normally recommended sync mode.

Schneider Electric Nigeria