{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Unable to assign an IP address to a Unity Momentum processor using a Bootp or DHCP server
Issue
The purpose of this resolution is to inform users of the Unity Momentum processors that an issue exists when attempting to assign an IP address.

When a new 171CBU9809x is powered up, right out of the box, it does not send out any bootp requests.  After the PLC is powered on and it completes its boot up routine, the 'ETH STS' LED immediately blinks 6x (operating using default IP address).  Therefore, no IP was assigned via a bootp or DHCP server.  The only method to assign an IP address was to manually load a configuration to the PLC via USB with an IP address configured.

The issue occurs with 171CBU9809x firmware v.1.00 and v1.20.



Product Line
171CBU98090
171CBU98091


Resolution
The issue was resolved in firmware version 1.21.


Schneider Electric Nigeria