{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATS01 be used on a Capacitance Start motor?

Issue:
Wondering If the ATS01 can be used on a Capacitance Start motor

Product Line:
All ATS01 soft starts

Environment:
ATS01 Soft Starts

Cause:
Capacitance Start motor on ATS01 soft starts

Resolution:
As noted in the catalog, the ATS01...FT models can be used with capacitor start single phase motors.  There is one caution: A long ramp up time can be detrimental to the motor capacitor. Contact the motor manufacturer to determine compatibility and ramp up time restrictions.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)


Schneider Electric Nigeria