Issue:
Remote mounting kit VW3A1102 specifications
Product Line:
ATV61, ATV71, ATV212, ATV32, ATV312
Environment:
Any drive that uses the VW3A1101 keypad
Cause:
None
Resolution:
VW3A1105 RJ-45 female—female adaptor is used to connect the LCD Graphic keypad and cable. It is not required if using VW3A1102.
Remote mounting kit VW3A1102 specifications
Product Line:
ATV61, ATV71, ATV212, ATV32, ATV312
Environment:
Any drive that uses the VW3A1101 keypad
Cause:
None
Resolution:
VW3A1105 RJ-45 female—female adaptor is used to connect the LCD Graphic keypad and cable. It is not required if using VW3A1102.
Released for:Schneider Electric Nigeria