{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Bandwidth limitation on the Ethernet Backplane
Issue

What is the specification on the Ethernet Backplane?

Product Line

M580


Resolution

The maximum throughput is 100 Mbits, full-duplex. So in theory, it's possible to push 100 Mbits in each direction (into the backplane and out of backplane).

However, to protect the backplane, the amount of traffic each module on the backplane can generate (CPU, NOC, etc.) is limited…see the user manual for each module. For instance the limitation is 7.6% for the NOC

Schneider Electric Nigeria