{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Changes in the LED color scheme from multi color to Green color for model references DM6100, DM6300, EM1000, EM1200 & EM1220

With effect from 6th Oct 2015, meter, all the meters from Sachetan local family bearing model reference number DM6100, DM6300, EM1000, EM1200 & EM1220 are being produced with Green color LED's for line indication at the front facia of the product. Prior to this change meter had provided multi color LED's (L1-Red, L2-Yellow & L3 - Blue) for the line healthiness application.

The main application of having multi color LED's are to indicate the presence of respective phase (s) across 3 phase electrical network. However with the mono color (Green) LED;s we can continue to achieve the similar objective as the 3 LED's across L1, L2, L3 location will lit up in the presence of 1 or 2 or 3 phase availability

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: