{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How can the type of stop be changed for the ATV312 (or ATV31) drive?

Article available in these languages: Finnish

The default setting for Type of Stop on the ATV312 drives is Ramp stop.

The options for stopping are:

  • Ramp
  • Freewheel
  • Fast Stop
  • DC Injection.

Programming below is showing the drive code and in brackets, (text using the VW3A1101 remote HMI display)
To access the Stop Mode, go to the FUn- (Application function) menu, then StC- (Stop Mode) then Stt (Type of stop).  The options are:
- rNP (Ramp)
- FSt (Fast stop)
- nSt (Freewheel)
- dCI (DC Injection)

Please note that nSt (Freewheel), FSt (Fast stop) and dCI (DC Injection) can also be assigned to other logic inputs under the StC- (Stop Modes) menu.

Schneider Electric Nigeria

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: