{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the remote keypad for the ATV32 variable speed drive?
Issue:
Part number for the remote keypad of ATV32 drive.

Product Line:
ATV32

Environment:
All

Cause:
Product Selection

Resolution:
​There are three keypad options for the ATV32 drives.

Option 1
VW3A1101 is an LCD keypad display.
VW3A1102 is the remote mounting kit with bezel providing IP54 rating.
VW3A1103 is an optional clear door providing IP65 rating and tamper resistance.
A cable is offered in several lengths:
VW3A1104R10 for a 1 meter cable.
VW3A1104R30 for a 3 meter cable.
VW3A1104R50 for a 5 meter cable.
VW3A1104R100 for a 10 meter cable.

Option 2:
VW3A1006 is a 4 digit LED keypad display rated IP54.
Use a cable from option 1 above.

Option 3
VW3A1007 is a 4 digit LED keypad display rated IP65.
Use a cable from option 1 above.

Schneider Electric Nigeria