{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
does we have Steel enclosure with sheet thickness 2mm ?
We don't have in our offer the mentioned dimensions with thickness of sheet metal = 2 mm. Yet the IK, degree of protection =IK10 conforming to IEC 62262 (impact energy 20 J (40 cm , 5KG)).
So this guarantee the mechanical withstanding and we don't have any needs to have thickness = 2mm.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.