{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the replacement for the Magelis XBTGT4230 HMI?

Issue
Replacement for Magelis XBTGT4230

Product Line
Magelis XBTGT

Cause
Obsolete

Resolution
The Magelis XBTGT4230 HMI can be replaced by either the HMIGTO4310 or (HMIDT351 + HMIG3U). Here are details for the substitution replacements:

Substitution of XBTGT4230 to HMIGTO4310:
---VijeoDesigner applications  are 100 % compatible.
---The cut-out is identical
---The communication ports are identical except on COM1 , no RS422-RS485 signal only RS232C. For RS422-RS485 link , use a cables with converter like TSXPCX1030 for Schneider Twido/Premium PLC or HMIZ951 for Mitsubishi FX PLC
---Same  certifications.
---No extension Bus for Fieldbus modules ( Profibus , DeviceNet , CANopen )
---No support of SoMachine PLC functions
---No auxiliary interface for speaker or alarm output
---Better Screen color TFT LED 65K , More Flash Memory , addition mini-USB Device port and use of SD card  slot.

OR

Substitution of XBTGT4230 to HMIDT351 + HMIG3U
---VijeoDesigner applications  are 100 % compatible.
---The cut-out is different , use of  HMIZGCO1 mechanical adaptor
---The serial communication ports are identical  but COM1 Subd9 RS422/R232C becomes the COM2 and the COM2 RJ45 RS485 becomes the COM1
---Ethernet port with higher speed and with a second port
---Same  certifications.
---Possible Extension Bus for Fieldbus modules ( Profibus , DeviceNet , CANopen )
---No support of SoMachine PLC functions
---Same auxiliary interface for speaker or alarm output
---Better Screen color TFT LED 262K and more resolution WVGA , More Flash Memory , addition mini-USB Device + Host USB ports and use of SD card  slot.

Schneider Electric Nigeria