{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What type of Communication Modules are available for the SEPAM Relays?
Product Line    
SEPAM Communications

Environment    
Networking and communications

Resolution  
The protocols that are available are:  DNP3, Modbus RTU, IEC 60870-5-103, Modbus TCP/IP, and IEC61850.  Not all modules have the same type of protocols or type of communications.  Attached is the communication accessory selection guide to help pick the correct module.  

Schneider Electric Nigeria

Attachment(s)
Communication Selection Guide.pdf [109.74 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top