Search FAQs
Video: Why won't the ATV630 drive run in reverse?
Issue:
ATV630 won't operate in reverse.
Product line:
ATV600, ATV630, ATV650, Altivar Process
Environment:
All
Cause:
Configuring Reverse Motor Operation on Altivar 630 Process Drives
Resolution:
The Factory settings for the Process Drive to run in reverse is not allowed.
To allow Reverse operations:
Go to Complete Settings > Command and Reference > Reverse Disable, change the setting from Yes (meaning Reverse is not allowed) to No (meaning Reverse is allowed) and save. Now, you should be able to operate the drive in Reverse.
ATV630 won't operate in reverse.
Product line:
ATV600, ATV630, ATV650, Altivar Process
Environment:
All
Cause:
Configuring Reverse Motor Operation on Altivar 630 Process Drives
Resolution:
The Factory settings for the Process Drive to run in reverse is not allowed.
To allow Reverse operations:
Go to Complete Settings > Command and Reference > Reverse Disable, change the setting from Yes (meaning Reverse is not allowed) to No (meaning Reverse is allowed) and save. Now, you should be able to operate the drive in Reverse.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: