Search FAQs
Is It essential to use the external neutral sensor TCE with Micro logic trip unit "6" for Masterpact ACB of types NT and NW ?
Kindly be informed that the external neutral sensor of type "TCE" is essential to be used with Masterpact ACB of types NT or NW in Micrologic trip unit "6" if the CB is of 3 poles
while it is not used if the NT or NW ACB is 4 poles
while it is not used if the NT or NW ACB is 4 poles
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: