{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Main function of UA or BA control units for Automatic transfer switch ATS using MCCB ?

The UA or BA controllers are used to control the operation truth table for an automatic transfer switch system (1 out 2),

they provide all the scenarios of breakers "which CB will operate and which will be opened during different operational conditions"

This is to keep the trasfering function fully automated between the two CBs

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: