{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to change Units in the ATV Process Drive?
Issue:
Adjust the units in the ATV Process drive.

Product Line:
Altivar Process
ATV6xx
ATV9xx

Environment:
All part numbers

Cause:
Default units  (Pressure in Bar, Flow in M3/h. Temp in deg C, Currency in Euro) may not be applicable to all customers in all regions of the world.

Resolution:
Using the HMI:
Under Menu 5 :[Complete settings], and subMenu 5.3 [Define system units] these settings can be manually changed.
To change using SoMove - See attached PDF.

Schneider Electric Nigeria

Attachment(s)
How to Change units in SoMove.pdf [50.35 KB]