{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why do I need to add "*" to my Alarm filter after upgrading from PLSCADA 7.20?

Issue
After upgrading from PLSCADA 7.20 or before, user now needs to add the wild character "*" to search for generic alarms.

Example:
In PLSCADA 7.20, user could search for all sags by typing in "sag" (without quotes) in the filter.
In Power SCADA Expert (PSE) 7.30 and above, user will need to type in "*sag" (without quotes) to get the same result.

Product
Power SCADA Expert 7.30 and above
PLSCADA 7.20 and below

Environment
OS supported by PLSCADA or PSE software

Cause
Changes to the alarming engine now require the "*" to be prepended to the string the user is filtering on.

Resolution
User must now prepend "*" to any filter if the word being filtered is not the first word in the alarm.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: