{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to assign a logic input to external fault on the ATS48?
Issue:
Assigning a logic input to external fault on the ATS48.

Product Line:
Altistart 48

Environment:
All Serial Numbers

Cause:
Logic input programming

Resolution:
To assign a logic input to external fault do the following:
From RDY
Press down to IO Menu,   press enter
Press down to LIx (3 or 4), press enter
Press the down arrow to LIE (external fault), press enter
ESC back to RDY

When the logic input goes active to 24Vdc, the ATS48 will go to a faulted state and display EtF.  After the logic input goes inactive to 0Vdc, a fault reset is required.

Schneider Electric Nigeria